How to Make a Linear Actuator Move Faster
By Shizu Yamaguchi Here, we’ll cover two ways to increase the speed of your linear actuator. But first, note that the linear actuators referred to in this article are known as slide tables and...
By Shizu Yamaguchi Here, we’ll cover two ways to increase the speed of your linear actuator. But first, note that the linear actuators referred to in this article are known as slide tables and...
By Florian Schiller Frost, ice and snow collecting on critical surfaces of an aircraft can quickly compromise safety. Any amount of buildup impairs an aircraft’s aerodynamics and in the worst case, can cause stalling...
By Shizu Yamaguchi In this article, we will define self-aligning plain bearings, cover how they came to be, go through their material makeup, design, and applications, then conclude with some things to think about...
By Nicole Lang There has been a monumental shift toward material handling or logistics robots (such as AGVs like the one pictured below) to help warehouses run smoothly and efficiently, . However, to ensure...
By Sebastian Bloechl Constantly increasing costs are forcing product development towards innovative alternatives. This is where value engineering (VAVE) comes in. What is VAVE, and how can it be used? VAVE is an effective...
By Shizu Yamaguchi Introduction What do you think of when you hear the word plastic? Cheap water bottles, maybe? Ripped plastic grocery bags? If so, you’re not alone. But what some people don’t realize...
By Max Herrmann Have you ever wondered why most cable conductors are made of copper and not another conductive material, like silver, gold or aluminum? And what’s up with gold-plated plugs? Read on to...
By Richard Habering Plain bearings often have to withstand heavy loads such as abrasive dust, high speeds or chemical loads in extreme environments. Last year, igus® developed an intelligent bearing – i.Sense – with iglide® high-performance...
By Katharina Esch Cables are frequently designed with PVC or PUR outer jackets. In addition to those, igus® uses TPE (thermoplastic elastomers) materials. TPE is a very robust material that we use in high-end cables meant for challenging applications....
By Avory Brookins Photo: “201014-N-RG482-0033” by Navy Medicine, licensed under Public Domain Mark 1.0 The COVID-19 pandemic has sparked an increase in demand for UV disinfection robots, which use ultraviolet radiation to kill germs in the air and/or...