- Efficient Energy Supply Systems for Cranes in Steel Plants White Paper
Read this white paper to learn about the benefits of switching to e-chain® cable carriers as an alternative to festoons for indoor cranes in steel plants.
- History of 3D Printing White Paper
Learn about the history of 3D printing — including recent innovations to existing methods and new methods altogether — with this ebook.
- The IIoT – Establishing a digital connection between industrial machines
As the world becomes more closely connected through the internet, industrial machines/technology need to keep pace. The IIoT not only makes this possible, but easy to do. This white paper will examine exactly how...
- The True Cost of Bearing Lubrication White Paper
In this white paper, learn about a simple solution that can have a positive, long-term impact on profitability for OEMs and their customers: the elimination of bearing lubricant. Further explore the hidden costs of...
- Plain bearing materials comparison: iglide® versus conventional plastics White Paper
In contrast to a few years ago, people today ask themselves less and less whether they should replace a metal plain bearing with a plastic one. Plain bearings made of plastics or plastic compounds...
- When to use plastic linear bearings and linear guides or recirculating ball systems White Paper
Linear bearings are machine elements that perform a linear movement. Rolling or sliding elements transmit the forces that occur. In this white paper, two linear guide concepts are compared: sliding on plastics as well...
- Influence of vibration on machine tools: Vibration behavior of e-chain systems® White Paper
The requirements for precision of machine tools are constantly growing. Their increasing automation gives specific challenges; for example, the influence of the vibration of machine components on the finished workpiece is an important factor...
- Cable management under adverse conditions: e-loop® as a versatile problem solver White Paper
A power and signal supply system for heavy-duty applications is an example of the creativity of design engineers and how quickly they implement their ideas in the heavy machinery industry. Originally developed for a...
- From the robot dress pack revolution to abrasion-free cleanroom chains to heavy-duty chains with extended service life White Paper
Today, e-chain® cable carriers are a standard machine part throughout automation technology. Their application spectrum is similarly broad–from semiconductor manufacture in cleanrooms to container cranes. As varied as chains are, there are technology trends...
- Toothed belt drive or lead screw drive: How do I choose the right linear actuator? White Paper
In the area of automation and mechanical engineering, linear axes are important elements that can be used for simple positioning tasks or for the implementation of complex, high-precision multi-axis systems. Linear actuators and linear...
- The Rise of Low Cost Automation E-Book
Automation is booming. What do you need to know to keep ahead of the curve? Read this detailed guide addressing trends in industrial robots and get informed about different low-cost automation products such as...
- Automation and Robotics for a (Cost-Effective) Fixed Price, From Product to the Platform: the igus® RBTX Marketplace White Paper
Looking for an automation solution, but hesitant to shell out the money for expensive components and software? The RBTX marketplace offers the ideal solution, providing automation components, software and complete systems from numerous different...
- Breaking the Injection Mold White Paper
How do the wear rates for 3D printed components fare compared to injection molded components? Get the data you are looking for in this detailed white paper. Other topics covered include a primer on...
- How Smart Plastics Decrease Plant Downtime White Paper
How can smart plastics as applied in cable carriers decrease plant downtime? In this detailed white paper, learn about predictive maintenance, the advantages of this implementation, in addition to its development from condition monitoring...
- Plastic Bearings Tolerances Assembly White Paper
What are the most important influencing factors to consider when determining the tolerance or fit of plastic plain bearings? Delve deep into this topic, along with how to measure and install plain plastic bearings...
- Robotic Cable Management Made Easy White Paper
You may think that moving from unprotected cables, using solutions like duct tape or corrugated tubing to a 3-dimensional robotic cable carrier is unnecessary but think again. In this detailed white paper, learn how...
- Small Mark, Huge Effect: CE White Paper
CE is a voluntary commitment to safety provided by suppliers that can give customers a reason to trust their components. Before affixing the marking, machine and system manufacturers go through an extensive, painstaking conformity...
- Plastic Plain Bearings: Tolerances, Assembly, Measurement White Paper
By Sherill Letourneau Read this whitepaper to learn everything you’ll need to know about our iglide® plain plastic bearings in regards to tolerance, assembly, measurement and more!
- drylin® E7 Plastic Linear Plain Bearings vs. PTFE-Lined Plain Bearings White Paper
Linear plain bearings are becoming commonplace in today’s manufacturing industry. As technologies and material sciences have advanced, so have the capabilities of linear plain bearings, particularly those made of plastic. This whitepaper will compare...
- Energy Supply Systems and Cables for Hygienic Applications White Paper
Given the extreme cost of cleanroom environments, even a very small foreign particle can ruin a chip and reduce yield in a cleanroom environment, as well as make the entire production uneconomical. Under these...
- Triple E-Class Container Ships and the Requirements for STS Cranes White Paper
What are the trends and challenges faced when loading and unloading today’s container ships with STS cranes? Read this detailed white paper to find out how modern demands are handled, how different energy supply...
- The ACME Lead Screw System White Paper
One of the most common lead screw geometries in North American manufacturing is the ACME lead screw system. Designed with a trapezoidal shape, a flank angle of 29 degrees and a higher pitch than fastening...
- e-spool: The Next Generation of the Cable Reel White Paper
Why e-spool and how is it designed? Starting with these simple questions about this innovative alternative to traditional cable reels, this white paper addresses how slip rings can be eliminated, relevant applications and industries,...
- Reducing Vibration of Cable Carriers on High Precision Machinery White Paper
In a number of industries, including printer design, semiconductor manufacturing and machine tools, cable carrier systems can be a possible source of vibration. How can vibration-reducing components be designed and how do these parts...
- Maximizing Shaft and Bearing Lifetimes in Agricultural Machinery White Paper
One of the most common causes of downtime and failure of agricultural machinery consists of wear on the machinery’s bearings and shafts. How do different shaft surface treatments reduce corrosion and wear? See the...
- The Less is More Approach to Robotic Cable Management White Paper
How robot cables are attached and guided on six-axis robots is important. Learn why, in addition to why the less is more approach to cable management has been taken on by many robotics engineers...
- Plastic Bearings Have Staying Power White Paper
Plastic bearings are strong enough to outperform and outlast metal in countless applications. However, they are often not considered a viable choice in the engineering community due to the common misconception that plastic is...