Why Flexible Cables Fail in Motion Applications: Rethinking How We Evaluate “Flexibility”

By Shizu Yamaguchi

In motion applications, cable failure is often attributed to product quality or supplier limitations. In reality, the root cause is usually more fundamental. It lies in how cables are evaluated during the design phase.

Terms such as “high flex” and visible characteristics such as how easily a cable bends are frequently used as indicators of suitability. These signals are intuitive, but they are incomplete. When applied without deeper context, they can lead to mismatches between cable construction and application demands.

This article examines how those mismatches occur. It reframes common evaluation approaches by looking at four areas: the difference between pliability and fatigue resistance, the distinction between installation and dynamic flex, the inconsistent use of the term “high flex,” and the role of motion profiles in determining performance.

The goal is to provide a clearer framework for selecting cables in continuous motion systems, where long-term reliability depends on aligning measurable properties with real operating conditions.

Pliability vs. Fatigue Resistance

A common starting point in cable evaluation is physical handling. If a cable bends easily, it is often assumed to be well suited for motion. This assumption is understandable, but it places too much emphasis on pliability.

Pliability describes how easily a cable can be bent in a static context. It is influenced by outer jacket material, strand flexibility, and overall construction. This characteristic is valuable during installation, particularly in constrained layouts. However, it does not indicate how the cable will behave under repeated motion.

Fatigue resistance, by contrast, describes how a cable performs under cyclic stress. In continuous motion systems, cables are subjected to repeated bending over defined radii. Each movement introduces small mechanical stresses that accumulate over time. The internal construction of the cable determines whether it can withstand this cycle count without degradation.

The distinction is subtle but important. A cable can be easy to bend once and still fail quickly under repeated motion. Evaluating cables based on how they feel during handling can therefore lead to overestimating their durability in dynamic applications.

A more reliable approach is to focus on performance data, including tested cycle life and construction details that are specifically designed for repeated motion.

Installation Flex vs. Dynamic Flex

Another source of confusion comes from how flexibility is described in specifications. Many cables are labeled as flexible, but the context for that flexibility is not always clear.

Installation flex refers to cables that can be bent during routing and installation. Once installed, these cables are expected to remain stationary. Their flexibility simplifies installation but does not indicate suitability for continuous movement.

Dynamic flex refers to cables designed for ongoing motion during operation. These cables are engineered to handle repeated bending, often within controlled environments such as cable carriers. Their performance is defined by measurable criteria such as cycle life and bend radius.

Problems arise when these two categories are treated as interchangeable. A cable that performs well during installation may not be designed for continuous movement. When used in dynamic applications, it may initially function as expected, but internal degradation begins early and progresses with each cycle.

Understanding this distinction helps prevent a common failure mode: selecting a cable that can be routed easily, but cannot sustain the motion it will experience over time.

The Challenge with “High Flex” as a Specification

The term “high flex” is widely used across the cable industry, but its meaning is not always consistent. In some cases, it indicates improved flexibility relative to a standard cable. In others, it is intended to suggest suitability for motion. Without a standardized definition, the term can be interpreted in different ways.

This variability creates risk during specification. Engineers may assume that “high flex” implies readiness for continuous motion, when in practice it may only indicate that the cable is easier to bend than a baseline product.

From an engineering perspective, qualitative labels are less useful than measurable parameters. Specifications that include defined bend radii, tested cycle counts, and environmental tolerances provide a clearer basis for decision-making. They allow engineers to match cable capabilities with application requirements more precisely.

The role of “high flex” can still be relevant, but it should be treated as a starting point rather than a final qualification. Additional data is needed to determine whether the cable is suitable for the intended motion profile.

Motion Profiles as the Defining Factor

Even when a cable is appropriately categorized, its performance ultimately depends on the conditions it experiences in operation. Motion profiles define those conditions, and they vary significantly across applications.

Cycle count is often the most important factor. A cable that performs reliably over a limited number of cycles may not be suitable for applications requiring continuous operation over millions of cycles. This difference is not always apparent at the specification level, but it becomes evident in service life.

Acceleration and deceleration introduce additional stress. Rapid changes in speed create inertial forces that act on both the cable and its internal conductors. These forces can accelerate fatigue, particularly when combined with high cycle counts.

Bend radius is another key variable. When cables are installed below their minimum specified radius, stress is concentrated in a smaller area, increasing the rate of degradation. Tight routing constraints can therefore reduce cable life if not accounted for during selection.

In some applications, torsion must also be considered. Twisting motion places different demands on cable construction than bending alone. A cable designed for bending may not be suitable for torsional movement unless explicitly rated for it.

These factors illustrate a broader point. Cable performance is defined less by general descriptors and more by how well the cable aligns with its specific operating environment.

Conclusion

Cable failure in motion applications is seldom unpredictable. It is usually the result of evaluating cables based on incomplete or misleading indicators.

Pliability can be mistaken for durability. Installation flexibility can be confused with dynamic capability. The term “high flex” can be interpreted without sufficient supporting data. At the same time, motion conditions such as cycle count, acceleration, and bend radius may not be fully accounted for during selection.

A more reliable approach is to evaluate cables based on measurable performance criteria and to align those criteria with the demands of the application. This shift does not require new principles, but it does require greater precision in how familiar concepts are applied.

Practical Checklist for Continuous Motion Applications

When selecting or evaluating cables for motion systems, engineers should confirm:

  • Flexibility is being evaluated correctly
    Distinguish between ease of bending and resistance to cyclic fatigue.
  • The intended type of flex is clearly defined
    Ensure the cable is designed for dynamic motion rather than installation-only flexibility.
  • Specification terms are supported by measurable data
    Look beyond “high flex” to cycle ratings, bend radius, and testing conditions.
  • Bend radius requirements are met in the actual design
    Confirm that routing stays within specified limits.
  • The full motion profile is considered
    Include cycle count, speed, acceleration, and travel distance.
  • Additional stresses such as torsion are addressed where relevant
    Verify that the cable construction matches all modes of movement.
  • Application conditions are reflected in the selection process
    Consider environment, layout, and mechanical constraints as part of the overall system.

Manufacturers that provide validated test data and application guidance, such as igus through its chainflex testing programs support this process by giving engineers a clearer basis for decision-making.

In continuous motion systems, reliability is achieved not by selecting a cable that appears flexible, but by selecting one that is proven to perform under the exact conditions it will face.

You may also like...

Leave a Reply